WHEN.PLCMD
Description
Records the value of PL.CMD when the when-condition is satisfied. The when-condition is checked once per 250 microseconds.
General Information
|
Type |
R/O |
|
Units |
Position units |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
Integer |
Variants Supported
This parameter is only supported on AKD BASIC drives.
Fieldbus Information
|
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? |
Object Start Version |
|---|---|---|---|---|---|
|
Modbus |
1174 |
Yes | 64 bit | No |
M_01-05-11-000 |
Related Topics